MLBlkCreate
Function - Creates a new Pipe Block object.
- Before a Pipe Block is Initialized, the function needs to be created and assigned an ID number.
- The MLBlkCreate function is automatically called if a Block is added to the Pipe Network.
-
-
- Pipe Blocks are normally created in the Pipe Network using the graphical engine.
- You do not have to add MLBlkCreate function blocks to their programs.
- The code with MLBlkCreate commands are automatically generated and called in a program with Pipe Network(MLPN_CREATE_OBJECTS).
-
-
This function should be called after MLMotionInit is called and before MLMotionStart is called.
Inputs
|
Input |
Data Type See Data Types. |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
Name |
STRING |
No range |
N/A |
No default |
Designated name for the newly created Pipe Block. |
|
Type |
STRING |
No range |
N/A |
No default |
|
Outputs
|
Output |
Data Type See Data Types. |
Range |
Unit |
Description |
|---|---|---|---|---|
|
ID |
DINT |
No range |
N/A |
Assigned ID number of the created Block. |
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
//Create a new GEAR Pipe Block named “MyGear”
MyGear := MLBlkCreate( 'MyGear', 'GEAR' );
See Also
- MLAxisInit
- See Step 3 in Initialize and Start a Pipe Network.