MLBlkReadOutVal

Pipe Network motion icon

 Function - Gets the output value of a selected Pipe Block.

Inputs

Input

Data Type

See Data Types.

Range

Unit

Default

Description

ID

DINT

1 to 1024

N/A

No default

ID number of a created Pipe Block.

Outputs

Output

Data Type

See Data Types.

Range

Unit

Description

Value

LREAL

No range

User units

Current output value of the selected Pipe Block.

FBD Language Example

FFLD Language Example

IL Language Example

Not available.

ST Language Example

//Save the output of a Gear Pipe Block 
BlockOutput := MLBlkReadOutVal( PipeNetwork.MyGear );

See Also