MLPrfReadIOffset

Pipe Network motion icon

 Function - Returns the Input Offset value of a selected CAM Profile.

  • Offsets can be changed on the fly to modify the CAM Profile while maintaining its shape.
  • A change in input offset is equivalent to shifting the CAM Profile on the X or Input Axis.

Figure 1: MLPrfReadIOffset

Inputs

Input

Data Type

See Data Types.

Range

Unit

Default

Description

ProfileID

DINT

1 to 1024

N/A

No default

ID number of a created CAM Profile.

Outputs

Output

Data Type

See Data Types.

Range

Unit

Description

OK

BOOL

No range

N/A

Offset

LREAL

No range

N/A

Returns the Input Offset of the selected CAM Profile.

FBD Language Example

FFLD Language Example

IL Language Example

Not available.

ST Language Example

//Save value of input offset
CamOffset := MLPrfReadIOffset( Profiles.Profile_A );

See Also