MLPrfWriteIOffset

Pipe Network motion icon

 Function - Sets the Input Offset value of a selected CAM Profile.

  • Offsets can be changed on the fly to modify the CAM Profile while maintaining its shape.
  • A change in input offset is equivalent to shifting the CAM Profile on the X (or Input) Axis.

Figure 1: MLPrfWriteIOffset

Inputs

Input

Data Type

See Data Types.

Range

Unit

Default

Description

ProfileID

DINT

1 to 1024

N/A

No default

ID number of an initialized CAM Profile.

Offset

LREAL

No range

N/A

No default

Desired new value of Input Offset.

Outputs

Output

Data Type

See Data Types.

Range

Unit

Description

Default (.Q)

BOOL

FALSE, TRUE

N/A

FBD Language Example

FFLD Language Example

IL Language Example

Not available.

ST Language Example

//Change the value of input offset
MLPrfWriteIOffset( Profiles.Profile_A , 45 );

See Also