MLCompReadRef
Function - Returns the reference position of a comparator block.
- The Transition Flag of a comparator object turns TRUE if the input position to the comparator is greater or equal to the reference.
- The Comparator Transition Flag stays TRUE until it is reset.
Inputs
|
Input |
Data Type See Data Types. |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
BlockID |
DINT |
1 to 1024 |
N/A |
No default |
ID number of an initiated Comparator object. |
Outputs
|
Output |
Data Type See Data Types. |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Reference |
LREAL |
No range |
User units |
Returns the current reference position of the Comparator object. |
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
//Return the Comparator Reference value
CompRef := MLCompReadRef( PipeNetwork.MyComp );
See Also