MLCompWriteRef
Function - Sets the reference position of a comparator block.
- The Transition Flag of a comparator object turns TRUE if the input position to the comparator is greater or equal to the reference.
- The Comparator Transition Flag stays TRUE until it is reset.
- If the input ThroughZero is set to TRUE, system must cross zero and then the reference position before the Transition Flag is set.
- If ThroughZero is FALSE, Transition Flag is set immediately if the input pipe position is greater then or equal to the Reference value.
Figure 1: MLCompWriteRef
Inputs
|
Input |
Data Type See Data Types. |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
BlockID |
DINT |
1 to 1024 |
N/A |
No default |
ID number of an initiated Comparator object. |
|
ThroughZero |
BOOL |
FALSE, TRUE |
N/A |
No default |
|
|
Reference |
LREAL |
No range |
User units |
No default |
New reference position to set in the selected Comparator object. |
Outputs
|
Output |
Data Type See Data Types. |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Default (.Q) |
BOOL |
FALSE, TRUE |
N/A |
|
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
//Set the Comparator Reference value
MLCompWriteRef( PipeNetwork.MyComp , TRUE , 45 );
See Also