MLDerReadInModPos
Function - Returns the Input ModuloPosition of the derivator block.
Input ModuloPosition is defined to manage the periodicity (modulo) of the input values.
Example
If the input value increases each millisecond by one degree then the output value is 1000 degrees per second.
Suddenly, the input value skips from 359 to 0 (zero).
- Input ModuloPosition = 360, the output continues to indicate 1000 degrees per second.
- This indicates that rollover into the next period has been properly handled
- Input ModuloPosition = 1000, the output then indicates 359,000 degrees per second.
- This indicates that the input has incorrectly interpreted roll-over as a 359 degree move in one millisecond.
Figure 1: MLDerReadInModPos
-
-
The first calculation of a Derivator Pipe Block just after the pipe installation indicates 0 (zero) regardless of the initial input value.
Inputs
|
Input |
Data Type See Data Types. |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
ID |
DINT |
1 to 1024 |
N/A |
No default |
ID number of an initiated Derivator object. |
Outputs
|
Output |
Data Type See Data Types. |
Range |
Unit |
Description |
|---|---|---|---|---|
|
ModuloPosition |
LREAL |
No range |
User units |
Current Input ModuloPosition of the selected Derivator object. |
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
//save the current input MODULO_POSITION of a Derivator object
DerInputPeriod := MLDerReadInModPos ( PipeNetwork.MyDerivator );
See Also