MLDerInit
Function - Initializes an derivator object.
- Function is automatically called if a Derivator Block is added to the Pipe Network with user-defined settings entered in the Pipe Blocks Properties screen.
- Input ModuloPosition is defined to manage the periodicity (modulo) of the input values.
-
-
- Derivator objects are normally created in the Pipe Network using the graphical engine.
- You do not have to add MLDerInit functions to their programs.
- Parameters are entered directly in pop-up windows; the code is automatically added to the current project.
Figure 1: MLDerInit
Inputs
|
Input |
Data Type See Data Types. |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
BlockID |
DINT |
1 to 1024 |
N/A |
No default |
ID number of a created Pipe Block. |
|
ModuloPosition |
LREAL |
0 to 1.0x10300 |
User units |
No default |
Value of the period of a cyclic system expressed in User units.
Example: If the input value increases each millisecond by one (degree), then the output value is a thousand (degrees per second).
|
Outputs
|
Input |
Data Type See Data Types. |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Default (.Q) |
BOOL |
FALSE, TRUE |
N/A |
|
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
//Create and Initiate a Derivator object
MyDerivator := MLBlkCreate( 'MyDerivator', 'DERIVATOR' );
MLDerInit( MyDerivator, 360.0 );
See Also