MLMstRel
Function - Performs a relative move for a specified distance from the current position.
Inputs
|
Input |
Data Type See Data Types. |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
EN |
BOOL |
FALSE, TRUE |
N/A |
No default |
Enables the function or function block to be executed. |
|
BlockID |
DINT |
1 to 1024 |
N/A |
No default |
ID name of the Master Block. |
|
DeltaPos |
LREAL |
No range |
User units |
No default |
Relative distance to the move. |
Outputs
|
Output |
Data Type See Data Types. |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Default (.Q) |
BOOL |
FALSE, TRUE |
N/A |
|
FBD Language Example
FFLD Language Example
-
-
- A positive transition contact is required to start the FB.
- See FFLD Contacts.
IL Language Example
Not available.
ST Language Example
MLMstRel( PipeNetwork.MASTER, 750.0 );
See Also