MLPmpReadFstSpd

Pipe Network motion icon

 Function - Gets the FirstTravelSpeed parameter of a PMP block.

  • This parameter is used as:
    • The first of two speeds in an MLPmpRel function block.
    • The speed in an MLPmpAbs function block.

Inputs

Input

Data Type

See Data Types.

Range

Unit

Default

Description

BlockID

DINT

1 to 1024

N/A

No default

ID name of a PMP function block in the Pipe Network.

Outputs

Output

Data Type

See Data Types.

Range

Unit

Description

FirstTravelSpeed

LREAL

 

User units / sec

Present first travel speed of the PMP Pipe Network function block.

  • Value defined in the setup of a PMP block in a Pipe Network.
  • The value is entered in the FIRST_TRAVEL_SPEED field in the Parameter tab.

FBD Language Example

FFLD Language Example

IL Language Example

Not available.

ST Language Example

FirstSpeedValue := MLPmpReadFstSpd( PipeNetwork.PmpMaster )  ;

See Also