MLTrigWriteDelay

Pipe Network motion icon

 Function - Sets the time the trigger block uses to compensate for the delay introduced by the sensor that captures the triggering signal.

  • Allows the trigger block to calculate the exact moment at which a signal was triggered by the specified compensation.
  • The delay compensation should include drive processing time, sensor delay, and the communication latency through the EtherCAT network.
  • Electronic sensors are not able to respond immediately to a signal.
  • Sensors usually require a certain amount of time to process a change of state in their input signal.

Fast Homing - Inputs

See these topics:

Inputs

Input

Data Type

See Data Types.

Range

Unit

Default

Description

BlockID

DINT

1 to 1024

N/A

No default

Identifier of the trigger block.

Delay

LREAL

No range

Microseconds

No default

Reaction time of the sensor that the trigger block has to compensate.

Outputs

Output

Data Type

See Data Types.

Range

Unit

Description

Default (.Q)
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
MLTrigReadDelay