Motion / Pipe Network
The KAS-IDE function library contains Motion Library (ML) function blocks (FBs) used to integrate motion from a Pipe Network in a PLC program.
These are the ML function blocks:
|
Function |
Description |
|||
|
Block |
Manage the blocks: Create / activate. See Block. |
|||
|
Motion |
Prepare the physical motion part: init, reset, start, stop. |
|||
|
Pipe Block |
Manage each specific Pipe Block: Read / write parameters. The function blocks are: |
|||
|
Pipe Network |
Manage the Pipe Network: Create / activate. See Pipe. |
-
-
Pipe Network code is generated automatically by the compiler.
Do not try to modify it.
Example: Pipe Block Description