Jumps JMP JMPC JMPNC JMPCN
Remarks
A jump to a label branches the execution of the program after the specified label.
See Insert Jump for directions on how to add a jump to a label.
-
-
Backward jumps can lead to infinite loops that block the target cycle.
FBD Language Example
- In the FBD Language, a jump is
represented by a signpost containing the label name.
- The input of the signpost must be connected to a valid Boolean signal.
- The jump is performed only if the input is TRUE.
In this example, the TON block is not called if bEnable is TRUE.
FFLD Language Example
- In the FFLD Language, the Insert Jump symbol (
), followed by the target label name, is used as a coil at the end of a rung. - The jump is performed only if the rung state is TRUE.
- Each rung can begin with a label.
- Labels are used as a destination for jump instructions.
In this example, Network #6 is skipped if IN1 is TRUE.
IL Language Example
Not available.
ST Language Example
Not available.
See Also