RETURN RET RETC RETNC RETCN
Remarks
- When used within an action block of a SFC step, the RETURN statement jumps to the end of the action block.
FBD Language Example
- The return statement is represented by the <RETURN> symbol.
- The input of the symbol must be connected to a valid Boolean signal.
- The jump is performed only if the input is TRUE.
In this example, the TON block will not be called if bIgnore is TRUE.
FFLD Language Example
- The <RETURN> symbol is used as a coil at the end of a rung.
- The jump is performed only if the rung state is TRUE.
In this example, all the networks above 5 are skipped if ENABLE is FALSE.
IL Language Example
Not available.
ST Language Example
IF NOT bEnable THEN
RETURN;
END_IF;
(* the rest of the program is not executed if bEnable is FALSE *)
See Also