FlipFlop
Function Block - Flipflop bistable.
- The output is systematically reset to FALSE if RST is TRUE.
- The output changes on each rising edge of the IN input, if RST is FALSE.
Inputs
|
Input |
Data Type See Data Types. |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
IN |
BOOL |
FALSE, TRUE |
|
|
Swap command (on rising edge). |
|
RST |
BOOL |
FALSE, TRUE |
|
|
Reset to FALSE. |
Outputs
|
Output |
Data Type See Data Types. |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Q |
BOOL |
FALSE, TRUE |
|
Output. |
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
(* MyFlipFlop is declared as an instance of FLIPFLOP function block: *)
MyFlipFlop (IN, RST);
Q := MyFlipFlop.Q;
See Also