any_to_dint / any_to_udint

PLCopen motion icon

Operator - Converts the input to a 32-bit integer value.

  • The default is 32-bit.
  • Can be unsigned with any_to_udint.

Inputs

Input

Data Type

See Data Types.

Range

Unit

Default

Description

IN

ANY

 

 

32-bit

Input value.

Outputs

Output

Data Type

See Data Types.

Range

Unit

Description

Q

DINT

 

 

Value converted to a signed double integer (32-bit).

Q

UDINT

 

 

Value converted to an unsigned double integer (32-bit).

Data Type Outputs

  • For BOOL input data types, the output is 0 (zero) or 1.
  • For REAL input data type, the output is the integer part of the input real.
  • For TIME input data types, the output is the number of milliseconds.
  • For STRING input data types, the output is the number represented by the string or 0 (zero) if the string does not represent a valid number.

FBD Language Example

FFLD Language Example

  • In the FFLD Language, the conversion is executed only if the input rung (EN) is TRUE.
    • The output rung (ENO) keeps the same value as the input rung.

IL Language Example

Not available.

ST Language Example

Q := ANY_TO_DINT (IN);

See Also