any_to_time

PLCopen motion icon

Operator - Converts the input into a time value.

  • For BOOL input data types, the output is t#0ms or t#1ms.
  • For DINT or REAL input data type, the output is the time represented by the input number as a number of milliseconds.
  • For STRING input data types, the output is the time represented by the string or t#0ms if the string does not represent a valid time.

Inputs

Input

Data Type

See Data Types.

Range

Unit

Default

Description

IN

ANY

 

 

 

Input value.

Outputs

Output

Data Type

See Data Types.

Range

Unit

Description

Q

TIME

 

 

Converts the input into a time value.

FBD Language Example

FFLD Language Example

  • In the FFLD Language, the conversion is executed only if the input rung (EN) is TRUE.
    • The output rung (ENO) keeps the same value as the input rung.

IL Language Example

Not available.

ST Language Example

Q := ANY_TO_TIME (IN);

See Also