MakeDWord

PLCopen motion icon

 Function - Builds a double word as the concatenation of two words.

Inputs

Input

Data Type

See Data Types.

Range

Unit

Default

Description

HI

USINT

 

 

 

Highest significant word.

LO

USINT

 

 

 

Lowest significant word.

Outputs

Output

Data Type

See Data Types.

Range

Unit

Description

Q

UINT

 

 

32-bit register.

FBD Language Example

FFLD Language Example

  • In the FFLD Language, the operation is executed only if the input rung (EN) is TRUE.
    • The output rung (ENO) keeps the same value as the input rung.
  • The function is executed only if EN is TRUE.
  • ENO keeps the same value as EN.

IL Language Example

Not available.

ST Language Example

Q := MAKEDWORD (HI, LO);

See Also