MakeWord

PLCopen motion icon

 Function - Builds a word as the concatenation of two bytes.

Inputs

Input

Data Type

See Data Types.

Range

Unit

Default

Description

HI

USINT

 

 

 

Highest significant byte.

LO

USINT

 

 

 

Lowest significant byte.

Outputs

Output

Data Type

See Data Types.

Range

Unit

Description

Q

UINT

 

 

16-bit register.

FBD Language Example

FFLD Language Example

  • In the FFLD Language, the operation is executed only if the input rung (EN) is TRUE.
    • The output rung (ENO) keeps the same value as the input rung.
  • The function is executed only if EN is TRUE.
  • ENO keeps the same value as EN.

IL Language Example

Not available.

ST Language Example

Q := MAKEWORD (HI, LO);

See Also