find

PLCopen motion icon

 Function - Find the position of characters in a string.

  • The first valid character position is 1.
  • The search is case sensitive.
  • The return value can be used with other string functions (e.g., mid or right).

Inputs

Input

Data Type

See Data Types.

Range

Unit

Default

Description

IN

STRING

 

 

 

Character string.

STR

STRING

 

 

 

Specific characters to search for within the STRING.

Outputs

Output

Data Type

See Data Types.

Range

Unit

Description

POS

DINT

 

 

  • Position of the first character of STR in IN.
  • Returns 0 (zero) if not found.

FBD Language Example

FFLD Language Example

  • In the FFLD Language, the operation is executed only if the input rung (EN) is TRUE.
    • The output rung (ENO) keeps the same value as the input rung.
    • The function is executed only if EN is TRUE.
    • ENO keeps the same value as EN.

IL Language Example

Not available.

ST Language Example

POS := FIND (IN, STR);

See Also