insert

PLCopen motion icon

 Function - Insert characters in a string.

The first valid character position is 1.

Inputs

Input

Data Type

See Data Types.

Range

Unit

Default

Description

IN

STRING

 

 

 

Character string.

STR

STRING

 

 

 

String containing characters to be inserted.

POS

DINT

 

 

 

Position of the first inserted character.

Outputs

Output

Data Type

See Data Types.

Range

Unit

Description

Q

STRING

 

 

Modified string.

FBD Language Example

FFLD Language Example

  • In the FFLD Language, the operation is executed only if the input rung (EN) is TRUE.
    • The output rung (ENO) keeps the same value as the input rung.
    • The function is executed only if EN is TRUE.
    • ENO keeps the same value as EN.

IL Language Example

Not available.

ST Language Example

Q := INSERT (IN, STR, POS);

See Also