FileClose
Function Block - Closes an open file.
Inputs
|
Input |
Data Type See Data Types. |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
Execute |
BOOL |
FALSE, TRUE |
N/A |
No default |
On the rising edge, request to close a file. |
|
ID |
UDINT |
No range |
N/A |
No default |
The ID of the open file. |
Outputs
|
Output |
Data Type See Data Types. |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Done |
BOOL |
FALSE, TRUE |
N/A |
If TRUE, the command completed successfully. |
|
Error |
BOOL |
FALSE, TRUE |
N/A |
If TRUE, an error has occurred. |
|
ErrorID |
DINT |
Enumerated |
N/A |
|
FBD Language Example
Not available.
FFLD Language Example
Not available.
IL Language Example
Not available.
ST Language Example
(* FileClose example *)
CASE StepCounter OF
0:
Inst_FileClose(TRUE, MyOutputFileID);
StepCounter := StepCounter + 1;
1:
Inst_FileClose(TRUE, MyOutputFileID);
IF Inst_FileClose.Done THEN
Inst_FileClose(FALSE, 0);
StepCounter := StepCounter + 1;
END_IF;
END_CASE;
See Also