FileDelete

PLCopen motion icon

 Function Block - Removes a file from the file system.

Inputs

Input

Data Type

See Data Types.

Range

Unit

Default

Description

Execute

BOOL

FALSE, TRUE

N/A

No default

On the rising edge, request to perform deletion of a file.

Path

STRING

No range

N/A

No default

The path to the file.

Outputs

Output

Data Type

See Data Types.

Range

Unit

Description

Done

BOOL

FALSE, TRUE

N/A

If TRUE, the command completed successfully.

Error

BOOL

FALSE, TRUE

N/A

If TRUE, an error has occurred.

ErrorID

DINT

Enumerated

N/A

FBD Language Example

Not available.

FFLD Language Example

Not available.

IL Language Example

Not available.

ST Language Example

(* FileDelete example *)
CASE StepCounter OF
0:
  Inst_FileDelete(TRUE, 'Test.txt');
  StepCounter := StepCounter + 1;
1:
  Inst_FileDelete(TRUE, 'Test.txt');
  IF Inst_FileDelete.Done THEN
     Inst_FileDelete(FALSE, '');
     StepCounter := StepCounter + 1;
  END_IF;
END_CASE;

See Also