Authentication and Access Control

Authentication ensures that only authorized users can make changes that affect system behavior.

Web Server Authentication

  • Configuration changes through the PCMM2G Web server are restricted to authenticated users with valid credentials.
  • User credentials are protected through secure password handling mechanisms.
    • Passwords are processed using salted cryptographic hashing prior to storage.
  • Stored credential data is maintained in a non-readable, one-way transformed format.
    • This prevents recovery of the original password value (even by Kollmorgen).
  • See User Authentication.

Authenticated KAS-IDE Access to PCMM2G

Engineering operations initiated from KAS-IDE include:

  • Project download.
  • Project start and stop.
  • Controller configuration modification require authentication using the existing PCMM2G Web server username and password.
  • See Connect to the Controller.

By default:

  • Authentication is required for KAS-IDE connections that perform protected actions.
  • Unauthenticated users cannot overwrite or control the active controller configuration.
  • An explicit configuration option is available to allow unauthenticated KAS-IDE access in controlled environments, with clear indication and warning of the reduced security posture.
    • See Security tab.
    • These mechanisms prevent unauthorized or accidental controller modification, even when users have network access or project files.