Connect to the Controller

KAS provides all the commands for controlling the target in the Device toolbar (Figure 1):

Figure 1: Device toolbar

Button

Description

Show the controller communication properties dialog box (Project Settings).

Change the controller IP address to connect with KAS Simulator.

Example: In this simulated mode, the controller properties change and the Controller Type includes the IP address 127.0.0.1. (Figure 2)

Figure 2: Controller Properties dialog box

See Using the KAS Simulator.

Compile the project.

Compile and download the project.

This downloads the application and Project Source files.

Establish a connection with the target controller.

An KAS Controller Login dialog box opens. (Figure 3)

Figure 3: KAS Controller Login dialog box

Close connection with the target controller.

Download the application to the targeted controller.

Start the application. It can be either:

  • Warm Start (default mode)
    • Retain Variables are loaded at the application startup.
    • They are Not re-initialized; whereas other variables are started with their initial values.
  • Cold Start
    • Use Retain Variables with their default values.
    • Cold starts occurs from time to time but are few.
    • To choose a Cold Start, click the Start button drop-down (Figure 4):
    • Figure 4: Start drop-down - Cold Start button

Stop the application.


  • If a previous download failed (due to the disconnected Ethernet or the controller is turned off), the application cannot be started.

    Additionally: 

    • No version information is shown in the web server or status bar.
    • The Start, Cold Start, and Download buttons are not available on the web server.

Click the button to verify the Simulated device mode is active.

Click the Connect Device button () to establish the connection with the target controller.

Actions to Prevent Compatibility Issues


    • The software versions of the KAS-IDE and the KAS Runtime are available in the local log messages (the level for this message is INFO).
    • See Information and Logs window.

When another KAS-IDE is already connected to the controller, a warning opens and the connection is discarded to prevent any conflict.

Application Status Bar

The status bar provides global information about the target and the name of the running application currently stored in the device.
Text with an orange background means that the version of the application is different between the KAS-IDE and the target.

See Status Bar.

Message Window

Every log message has this information:

  • Timestamp
  • ID
  • Message

  • Once connected to the device, it is no longer possible to edit the PLC programs, unless Online Change is active.
    See Compile the Project.

    • Depending on the number of Kollmorgen AKD Series Servo Drives physically present in the EtherCAT network, the KAS-IDE might slow down when getting data.
    • The KAS Runtime is not concerned with this limitation.