Download the Project
Click the Compile and Download (
) button (Ctrl + F7) or the Download (
) button.
The application is compiled and downloaded or just downloaded to the controller.
An alert appears if:
- An attempt to Compile and Download is made without a connection to a controller.
- There is not sufficient space on the controller for the application.
- Clearing the User Data tab is one method to create more space on the controller.
- In the Controller Properties dialog box, if the Download Project Source in the controller option is:
- Enabled - the source code is copied to the controller.
See Configure the Controller. - Disabled - and the controller has project source loaded, a message appears.
- The message is different based on whether the current project and the project on the controller have the same name or not.
- Enabled - the source code is copied to the controller.
Project Name - Same Name
If the Project Name is the same, the message is (Figure 1):
Figure 1: Download Project Source message - Project Name = Same Name
Actions
Click either:
- OK: Source on controller is deleted.
- Save: Source on controller is overwritten and is saved to "My Documents".
- If that source file already exists in My Documents, a prompt appears to rename the source file, overwrite that file or not.
- If the file is not renamed or overwritten, the download to the controller is canceled.
- Cancel: Download is stopped.
Project Name - Different Name
If the Project Name is different, the message is (Figure 2):
Figure 2: Download Project Source message - Project Name = Different Name
Actions
Click either:
- OK: Source on the controller is replaced.
- Save: Source on the controller is saved to My Documents.
- Cancel: Download is stopped.
-
-
The versions between the KAS-IDE and the KAS Runtime must be the same to debug the application.
Example: To view the Variable Animation in the editors.
-
-
If the KAS-IDE version differs from the KAS Runtime after compiling an application, the function blocks defined in the KAS-IDE and those implemented in the virtual machine of the runtime can be different.
To prevent this potential mismatch, compile and download the application again.
-
-
The project's source code can be downloaded to store the project.
See the File menu about retrieving saved projects.