Add the Controller

  1. Click the File menu and select New.
    The Create a New Projectdialog box opens. (Figure 1)
    By default, PCMM2G is selected as the Controller.
  2. Figure 1: Create a new project dialog box

  3. In the Choose an application template section:
    1. In the Template Type section, choose the motion engine option
      (Pipe Network Concept or PLCopen)
      .
    2. In the Template list box, select an application template.
      See the Available Application Templates list).
  4. Click Finish.
  5. Click the File menu and select Save As.
    The Save As dialog box opens.
  6. Define the Project Name and its location.
  7. Click OK to save the changes or selections and close the dialog box.

Available Application Templates