View the Controller IP Address

The IP address assigned to the controller is shown in the 7-segment display.

  • The IP address is shown at boot and can be accessed from the B3 Menu Button.
  • The default IP address depends on the Rotary Switch RS1 position.

Example


    • On the PCMM2G, if a network cable is not attached or no IP address is assigned, the controller shows an IP address of 0.0.0.0.