Using the Controllers
Tasks related to the Kollmorgen controllers are:
- Configure parameters.
- Start and stop the KAS application.
- Update the firmware.
- Reset to factory settings.
- Review of Controller Error and Alarm Descriptions.
Rebooting or resetting the controller and recovering the firmware can be performed from the device or using the Web server.