Backup and Restore from the Web server
The Backup and Restore functions are used to replicate a Kollmorgen controller.
The controller data is replicated on the PCMM2G USB flash drive.
These are the elements that are backed up or restored:
- Controller firmware.
- Date/Time - Network Time Protocol (NTP) and Set Time Zone settings.
- EtherCAT network topology.
- Kollmorgen servo drives firmware packages and their respective drive parameters.
- Network configuration.
- PLC Application.
- Retain Variables.
- Shared Directory settings.
- SSH Connection Enable/Disable configuration.
- User data files.
- See User Data tab.
- Web server and SSH user accounts configuration.
Restore Notes
- The drive's data and firmware are copied from the USB flash drive to the controller flash when the Restore Controller function is selected.
- The Restore EtherCAT Devices function should be selected for restoring the data and the firmware of any replaced Kollmorgen AKD Series Servo Drives.
-
-
- A PCMM2G backup created from any PCMM2G axis model can be restored on a different axis model.
- The restored KAS project does not run if the physical axes need for the project is more than the restored model can support.
The Backup and Restore processes:
- Cannot be performed while an application is running.
- Takes several minutes to complete.
- Do not power off the controller once started.
- The controller is rebooted after a Restore.
|
Backup File Source |
PCMM2G Restore |
|---|---|
|
PCMM2G Backup |
Yes |