Backup the Controller

This procedure is used to replicate a PCMM2G.

The backup is stored on the USB flash drive connected to PCMM2G.

These are the elements that are backed up:

  • Controller firmware.
  • Date/Time - Network Time Protocol (NTP) and Set Time Zone settings.
  • EtherCAT network topology.
  • Kollmorgen servo drives firmware packages and their respective drive parameters.
  • Network configuration.
  • PLC Application.
  • Retain Variables.
  • Shared Directory settings.
  • SSH Connection Enable/Disable configuration.
  • User data files.
  • Web server and SSH user accounts configuration.

Procedure

  1. On the Backup tab, click the Backup Controller button. (Figure 1)
  2. Figure 1: Backup Controller button

  3. A confirmation message appears to continue the backup. (Figure 2)
  4. Figure 2: Confirmation message

  5. Click OK to continue.

    • This operation cannot be performed while an application is running.
    • This operation may take several minutes.
    • Once started, do not power off the controller.

See Also

  • EtherCAT Devices Backup
  • PCMM2G Controller and EtherCAT Devices Backup