Controller Backup and Restore
The Backup and Restore functions are used to replicate a Kollmorgen controller.
The controller data is replicated on the PCMM2G USB flash drive.
Backup
Backup is performed using the web server.
- This is recommended because it has functionality the button method does not offer (e.g., back up the drive data).
-
-
For a complete backup of both the controller and drive, use the Web Server backup.
Restore
Restoring information to the controller is performed using the web server.
|
Backup & Restore What? |
PCMM2G To/From
|
PCMM2G To/From |
|---|---|---|
|
Controller: Firmware |
|
|
|
Controller: Network Configuration |
|
|
|
Controller: PLC Application |
|
|
|
Controller: Retain Variables |
|
|
|
EtherCAT Devices: AKD / AKD2G Drive Firmware |
|
|
|
EtherCAT Devices: AKD / AKD2G Drive Parameters |
|
|
|
EtherCAT Devices: Network Topology |
|
|
‡ Restore only
Data Transfer
- The 7-segment display shows chasing light animation while the backup or restore is occurring.
(repeats) - The Backup and Restore functions have an all-or-nothing behavior.
- PCMM2G: If there is no USB flash drive inserted, not enough space on the USB, or if files are missing, nothing is copied and the 7-segment display shows an error code.
- If files already exist on the USB flash drive (in the backup directory), they are deleted and replaced with the new backup configuration files.
- The files on the controller are replaced with the USB flash drive files.
-
-
- Do not modify the files on the USB flash drive.
- This could result in the restore function failing.
-
-
If there are multiple backup configurations, you must use one USB flash drive per backup configuration.