Backup and Restore tab
The controller can backup and restore EtherCAT devices on an EtherCAT network.
Figure 1: Backup and Restore tab
This feature:
- Is useful as a maintenance operation to replace any controller drives in an operational machine.
- Reduces the manual steps for saving/loading each drive’s firmware and parameters into a few automated steps.
The Backup/Restore functionality is located in the controller's Web server and is accessible from a web browser.
See Also
See the Controller Backup and Restore in the KAS-IDE help.