Upgrade the Controller's Firmware

This procedure is used to upgrade the controller's firmware using the web server.

  1. Identify the controller's IP address.
    See View the Controller IP Address.
  2. Open a web browser and enter the controller's IP address.
    The Web server KAS Home window opens. (Figure 1)
  3. Figure 1: KAS Home window

  4. Login to the controller.
  5. Click the Settings tab.
  6. Click the Firmware tab.
  7. Figure 2: Firmware tab - Upgrade Firmware area

  8. In the Firmware Information area, verify the Recommended file name for the upgrade file to download and use. (Figure 2)
  9. Examples:

    PCMM2G

    See these file naming convention topics:

  10. Open the applicable controller product web page:
  11. In the Software tab, under the Title column, locate the appropriate firmware upgrade file.
  12. Click the link for the upgrade file.
    The file automatically downloads to the location designated for the browser.
  13. Close the browser window.
  14. Return to the KAS the Firmware tab.
  15. In the Firmware Upgrade area, click the Choose File button. (Figure 3)
    A Windows Explorer window opens.
  16. Figure 3: Firmware Upgrade area

  17. Search for and select the firmware file downloaded in Step 9.
  18. Click Open to select the file an close the window.
  19. Click the Upgrade button to start the process.

    • If the Upgrade button is disabled, log into the Web server.
      Click Login at the top of the web page and enter the password.
      See User Authentication about logging in.

    A message and a throbber are shown across the web page, indicating that maintenance is in progress.

    The 7-segment display on the controller animates with chasing lights.


    • Do not refresh the web page until firmware upgrade is completed.
      If performing a boot loader upgrade, do not power-off or restart the PCMM2G until the boot loader upgrade is completed.

    Successful Upgrade: The controller automatically reboots with new firmware.

    When the reboot is complete, the user is logged out of the controller.
    The webserver displays a message to indicate the user has been logged out.

  20. Press <CTRL+F5> to force the controller's web browser to refresh the page.
    The new firmware version appears in the Firmware Information area.

See Also