AXIS#.TUNING.ISSLIDERINUSE
Description
AXIS#.TUNING.ISSLIDERINUSE indicates whether the current tuning solution was computed by the QuickTune feature or the Slider Tuning feature. This value also indicates if the keyword AXIS#.TUNING.BANDWIDTH is valid or not. If this value is 0, then a Bode measurement is needed to identify the velocity loop bandwidth.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-13-01-000 |
- |
General Information
| Type | Read Only |
| Units | N/A |
| Range | 0 - 1 |
| Default Value | 1 |
| Data Type | Integer |
| See Also | AXIS#.TUNING.BANDWIDTH |
| Stored in Non-Volatile Memory | No |
Variants Supported
All variants are supported.