Install KAS-IDE

System Requirements

These are the minimum system requirements for the KAS-IDE.

Component

Description

Supported Operating Systems

  • Microsoft Windows 11 (64-bit).
  • Microsoft Windows 10 (32-bit or 64-bit).
  • For optimal performance, verify the operating system is fully updated with the latest patches.

Connectivity

  • 1 Ethernet port or WiFi connectivity, at either 100 MB or 1 GB.
  • See Note #2.

Display

  • WXGA+ (1440 x 900) or higher-resolution monitor with 24-bit, 16.7M colors.
  • See Note #1.

Hard Disk

Free space required on hard disk:

  • 32-bit hard disk: 16GB
  • 64-bit hard disk: 20GB

Network

Internet connection for downloading and updating WebView2 Runtime.

Processor

Intel Pentium M or equivalent processor at 1.5GHz or greater.

RAM

  • 32-bit: 1GB RAM
  • 64-bit: 2GB RAM or greater
    • Recommended for complex applications.

Software

  • Microsoft Edge WebView2 Runtime (Evergreen) version 133.0.3956.59 or newer.
  • .NET Framework 4.8.1 or newer.

Web Browser

  • A modern web browser is required to access the controller Web server and online help.
  • We recommend Microsoft Edge.

    1. Better results are achieved with OpenGL and 3D cards.
    2. A 100MB or 1GB network is required to allow the KAS-IDE to Runtime communication to work in all conditions.
      The AKD WorkBench AutoTuner and Scope both require 100MB of bandwidth to function properly.


    • See Connect Remotely about the ports used by the KAS.
    • The ports may need to be opened to support connecting to a controller from an external network.

Digital Signatures

The KAS-IDE Installer and the executables are digitally signed to protect the integrity of these files and identify the distributor of the software components.

The digital signature appears as part of the file properties.

Figure 1: Example: KAS Setup Properties Digital Signature

Download

The latest version of the Kollmorgen Automation Suite is available from the Kollmorgen Support Network here: KAS IDE Distribution.


    • This is a restricted site.
    • You must be given access based on having purchased KAS.
    • If you do not have access, contact Support and Services.

Procedure

  1. Open the KAS IDE Distribution site.
  2. Login to the site.
  3. In the table, click the applicable Full or Small Installer link.
    The file starts downloading.
  4. When the download is completed, continue with the KAS-IDE Installation.

KAS-IDE Installation


    • Installation of the KAS-IDE can require you to change firewall settings.
    • If you do not have sufficient privileges to configure your firewall, you must stop the relevant Windows Service.

Procedure

  1. On the computer, locate the folder where the EXE file was downloaded to.
  2. Double-click the EXE file.
    The Kollmorgen Automation Suite Setup starts loading.

    • The Verified Publisher in the installation wizard dialog must be REGAL REXNORD CORPORATION.

  3. Wait for the setup splash screen to vanish after being displayed.
    The Kollmorgen Automation Suite Setup wizard starts.
    The Welcome window opens showing the version number of the KAS-IDE. (Figure 2)
  4. Figure 2: Welcome window

  5. Click Next.
    The License Agreement window opens. (Figure 3)
  6. Figure 3: License Agreement window

  7. Review the License Agreement and click I Agree.

    • You must accept the agreement to install KAS.

  8. The Choose Components window opens. (Figure 4)

    Figure 4: Choose Components window

  9. From the drop-down menu, verify the Development Environment installation type is selected.
  10. Click Next.
    The Choose Users window opens. (Figure 5)
  11. Figure 5: Choose Users window

  12. Select either:
    • Install for all users (Requires Administrative Privileges)
    • Install for current logged-in user (No Administrative Privileges Required)

    • Kollmorgen recommends installing for All Users if this is a first time KAS-IDE installation on the computer.

     


    • The KAS-IDE software requires these Windows components to be installed on your system:

      • .NET Framework 4.8.1 Runtime
      • WebView2 Runtime

      If these components are not already installed, the installer prompts you to install them.

      Administrative privileges may be required for the initial installation of these components.

  13. Click Next.
    The Choose Install Location window opens. (Figure 6)
  14. Figure 6: Choose Install Location window

  15. Accept the recommended default location.
    Option: Click Browse to specify a custom install directory.

    • Kollmorgen does not support non-ASCII characters in the install location path.

      If these characters exist in the path, you must specify a different installation directory.

     


    • Kollmorgen recommends accepting the default destination folder:

      • For the All Users option, the location is here:
        • C:\Program Files\Kollmorgen\Kollmorgen Automation Suite\Kollmorgen Automation Suite <<KAS-VERSION-ID>>.
      • For the Current User option, the location is here:
        • C:\Users\{{user.name}}\AppData\Local\Kollmorgen\Kollmorgen Automation Suite <<KAS-VERSION-ID>>.
  16. Click Next.
    The Choose Start Menu Folder window opens. (Figure 7)
  17. Figure 7: Choose Start Menu Folder window

  18. Accept the recommended default folder name.
    Option: Edit the text to specify a custom folder name.
  19. Click Install.
    KAS-IDE is installed in the designated install location.
    1. If WebView2 is not installed, the Figure 8 message appears.
    2. Figure 8: WebView2 Confirmation message

    3. Continue with WebView2 Installation.
  20. When the installation is complete, the Completing KAS Setup window opens. (Figure 9)

    Figure 9: Completing KAS Setup window

  21. Click Finish to close the wizard and open the Release Notes.

WebView2 Installation


    • The KAS software uses Microsoft WebView2 Runtime software to display the documentation and web server pages from the KAS-IDE.

Notes

  • If Microsoft WebView2 is NOT installed, the KAS-IDE installer prompts the user to download and install it from the Microsoft website here: Microsoft Edge WebView2 Runtime software.
  • Use either the Evergreen Bootstrapper or the Evergreen Standalone installers.
    • Do not use the Fixed version installers!
  • The user must follow the provided link to install WebView2 to view the documentation and access the web server from the KAS-IDE.

Procedure

  1. Click Yes.
    The Download area of the Microsoft Edge WebView2 website opens.
    • Use either the Evergreen Bootstrapper or the Evergreen Standalone installers.
      • Do not use the Fixed version installers!
  2. Download the applicable Evergreen installer.
  3. Click the Accept and Download link to the license terms and download the software.
  4. Locate and install the MicrosoftEdgeWebview2Setup.exe file.
    Wait until the installation process is complete.

User Data

  • User-generated data (e.g., log files, project sources, field bus configurations, function blocks, etc.) are stored in the Windows User directory and are maintained between installations.
  • This applies to files on PCMM2G and Simulator files.

Additional Literature

Document Title

Description

Release Notes

The KAS Release Notes contain a summary of:

  • New features, fixed and known limitations, workarounds
  • Information on all hardware and software components that have been updated, changed, or added in the release.
  • See KAS Release Notes EN.

Getting Started

Contains these main steps to get the KAS system up and running.

  • Hardware (HW) Installation (Connection and Wiring): Wiring and hardware details, connectors, system diagrams.
  • HW Configuration: Basic configuration and settings needed to start the HW components (e.g., HMI, Industrial PC, Fieldbus, I/O).
  • Software (SW) Installation: KAS software setup.
  • See KAS IDE Getting Started EN.

30 Minutes to Motion

Contains the main topics to get started quickly with KAS-IDE.

The objective is to familiarize you with the basic principles and the way the program works by creating a simple motion application project.

 

See KAS IDE 30 Minutes to Motion EN about:

KAS-IDE User Manual

Contains content to help with KAS-IDE except the topics included in the Reference Manuals.

See KAS-IDE User Manual EN.

KAS-IDE PLC Library Reference Manual

Contains Technical References on PLC Programming Languages and Library.

See KAS-IDE PLC Library Reference Manual EN.

KAS-IDE Motion Library Reference Manual

Contains Technical References on Motion Library for Pipe Network and PLCopen.

See KAS-IDE Motion Library Reference Manual EN.