Project Templates
KAS provides start up templates to help you get started.
See Add the Controller to use the project setup wizard.
These are the templates for the Pipe Network and PLCopen motion engines:
Coordinated Motion
|
Template Name |
Description |
|---|---|
|
|
|
|
|
KAS Runtime
|
Template Name |
Description |
|---|---|
|
Library |
Used to create a custom library. |
KDN Download
|
Template Name |
Description |
|---|---|
|
KDN |
Pipe Network
|
Template Name |
Description |
|---|---|
|
Simple initialization, relative position move. |
|
|
Simple initialization, relative position move. |
|
|
Position and velocity moves, gearing, camming, and drive status. |
|
|
Position and velocity moves, gearing, camming, and drive status. |
|
|
Position and velocity moves, gearing, camming, and drive status with optimized performance. |
PLCopen
|
Template Name |
Description |
|---|---|
|
Simple initialization, relative position move. |
|
|
Simple initialization, relative position move. |
|
|
Position and velocity moves, gearing, camming, and drive status. |
|
|
Position and velocity moves, gearing, camming, and drive status. |
|
|
Position and velocity moves, gearing, camming, and drive status with optimized performance. |
Template Inclusions
These templates come complete with software to:
- Create two or three axes of servo motion
- Enable the drives
- Perform simple motion
The templates contain variables which support these operations.
Additionally, the templates contain a Control Panel for ease of running motion.
-
-
The templates may need to be changed to run on specific hardware.