AIN#.OFFSET

Description

AIN#.OFFSET sets the analog offset, which is added to the analog input command to the drive. This value compensates for the analog input signal (AIN#.VALUE) offset or drift.

Examples

Code

--> AIN1.VALUE
0.056 V
--> AIN1.OFFSET -0.056
--> AIN1.VALUE
0.000 V 

Context

For more information see Analog Input.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type Read/Write
Units V
Range -10V to +10V
Default Value 0 V
Data Type Float
See Also  
Stored in Non-Volatile Memory Yes

Variants Supported

All variants are supported.

Fieldbus Information

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AIN1.OFFSET

3780h

05h

Signed16

-

1000:1

Read/Write

No

AIN2.OFFSET

3781h

05h

Signed16

-

1000:1

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

23050

1

23050 (0x5a0a)

AIN1.OFFSET

Signed16

Read/Write

Yes

23051

1

23051 (0x5a0b)

AIN2.OFFSET

Signed16

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AIN1.OFFSET

23050

Float

Read/Write

-

AIN2.OFFSET

23051

Float

Read/Write

-