AIN#.ZERO

Description

AIN#.ZERO causes the drive to zero the analog input signal (AIN#.VALUE). You may need to execute this command more than once to achieve zero offset.

Examples

Code

--> AIN1.VALUE
0.056 V
--> AIN1.OFFSET
0 V
--> AIN1.ZERO
--> AIN1.VALUE
0.000 V
--> AIN1.OFFSET
-0.056 V 

Context

For more information see Analog Input.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type Command
Units N/A
Range N/A
Default Value N/A
Data Type N/A
See Also  
Stored in Non-Volatile Memory No

Variants Supported

All variants are supported.

Fieldbus Information

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

23250

1

23250 (0x5ad2)

AIN1.ZERO

Unsigned8

Read/Write

No

23251

1

23251 (0x5ad3)

AIN2.ZERO

Unsigned8

Read/Write

No

PROFINET

Parameter

PNU

Data Type

Access

Units

AIN1.ZERO

23250

Unsigned8

Read/Write

-

AIN2.ZERO

23251

Unsigned8

Read/Write

-