AXIS#.IL.COMPTABLE.MAX

Description

AXIS#.IL.COMPTABLE.MAX sets the cogging compensation/torque compensation table index maximum. The table ends at the defined maximum axis position.

When AXIS#.PL.FB is equal to AXIS#.IL.COMPTABLE.MAX, the output of the table will be equal to the last table entry.


  • The units of AXIS#.IL.COMPTABLE.MAX is determined by the value of AXIS#.UNIT.PROTARY or AXIS#.UNIT.PLINEAR.

Example

To set the of the table to 360 degrees, the user would enter:

-->AXIS1.IL.COMPTABLE.MAX 360

Versions

Action Version Notes
Implemented 02-07-03-000

General Information

Type

Read/Write

Units

Rotary: counts, rad, deg, custom units, 16-bit counts

Linear: counts, mm, µm, custom units, 16-bit counts

See Position Units for details.

Range

Depends on units. See Position Range for details.

Default Value

360.0 Degrees

Data Type

Float

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.IL.COMPTABLE.MAX

500ah

1ah

Signed32

Position

-

Read/Write

No

AXIS2.IL.COMPTABLE.MAX

510ah

1ah

Signed32

Position

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

5839

1

5839 (0x16cf)

AXIS1.IL.COMPTABLE.MAX

Signed32

Read/Write

Yes

71375

2

5839 (0x16cf)

AXIS2.IL.COMPTABLE.MAX

Signed32

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.IL.COMPTABLE.MAX

5839

Signed32

Read/Write

Position