AXIS#.MOTOR.TEMPSOURCE
Description
This parameter selects the connector used for the motor temperature measurement when the axis motor control algorithm does not use a position feedback (when AXIS#.MOTOR.TYPE = 2 or 10). The temperature sensor is a thermal resistor connected to the drive through a 2-wire input. The type of thermal resistor is set with AXIS#.MOTOR.RTYPE.
The range of available AXIS#.MOTOR.TEMPSOURCE values are determined by the set of drive connectors. The connectors that support temperature measurements are full 15-wire connectors (X23) and Smart Feedback Adapter (SFA) devices (X1 and X2 with SFA).
When AXIS#.MOTOR.TYPE is not 2 or 10, AXIS#.MOTOR.TEMPSOURCE is not used.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-06-01-000 |
General Information
Type |
Read/Write |
Units |
N/A |
Range |
Depends on drive model |
Default Value |
1 |
Data Type |
Integer |
Stored in Non-Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
---|---|---|---|---|---|---|---|
AXIS1.MOTOR.TEMPSOURCE |
500bh |
23h |
Unsigned8 |
- |
- |
Read/Write |
No |
AXIS2.MOTOR.TEMPSOURCE |
510bh |
23h |
Unsigned8 |
- |
- |
Read/Write |
No |
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
---|---|---|---|---|---|---|
6244 |
1 |
6244 (0x1864) |
AXIS1.MOTOR.TEMPSOURCE |
Unsigned8 |
Read/Write |
Yes |
71780 |
2 |
6244 (0x1864) |
AXIS2.MOTOR.TEMPSOURCE |
Unsigned8 |
Read/Write |
Yes |
Parameter |
PNU |
Data Type |
Access |
Units |
---|---|---|---|---|
AXIS#.MOTOR.TEMPSOURCE |
6244 |
Unsigned8 |
Read/Write |
- |