AXIS#.PL.ERR

Description

AXIS#.PL.ERR is the position loop error when the axis is operating in position mode (AXIS#.OPMODE = 2). It is the difference between the commanded axis position and the measured position. If the axis is not operating in position mode, AXIS#.PL.ERR is set to 0.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read Only

Units

Rotary: counts, rad, deg, custom units, 16-bit counts

See Position Units for details.

Range

Depends on units. See Position Range for details.

Default Value

N/A

Data Type

Float

See Also

AXIS#.PL.FB

Stored in Non-Volatile Memory

No

Variants Supported

All variants are supported.

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.PL.ERR

60f4h

00h

Signed32

Position

-

Read only

Yes

AXIS2.PL.ERR

68f4h

00h

Signed32

Position

-

Read only

Yes

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

5901

1

5901 (0x170d)

AXIS1.PL.ERR

Signed32

Read Only

Yes

71437

2

5901 (0x170d)

AXIS2.PL.ERR

Signed32

Read Only

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.PL.ERR

5901

Signed32

Read Only

Position

Related Topics

AXIS#.PL.ERRFTHRESH | AXIS#.PL.ERRWTHRESH

"Position Loop"