AXIS#.VL.ERR

Description

AXIS#.VL.ERR is the velocity loop error. It is calculated in the velocity loop as the difference between AXIS#.VL.CMD and AXIS#.VL.FB .

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read Only

Units

Rotary: RPM, RPS, deg/s, (custom units)/s, rad/s

See Velocity Units for details.

Range

N/A

Default Value

N/A

Data Type

Float

Stored in Non-Volatile Memory

No

Variants Supported

All variants are supported.

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.VL.ERR

5011h

05h

Signed32

Velocity

-

Read only

Yes

AXIS2.VL.ERR

5111h

05h

Signed32

Velocity

-

Read only

Yes

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

6023

1

6023 (0x1787)

AXIS1.VL.ERR

Signed32

Read Only

Yes

71559

2

6023 (0x1787)

AXIS2.VL.ERR

Signed32

Read Only

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.VL.ERR

6023

Float

Read Only

Velocity