FB#.LINEPITCH

Description

This parameter defines the line pitch for linear encoders in nm per line. This is only used when using linear motor types. For rotary motors, see FB.ENCLINES.

Context

See Feedback # View and FB#.MECHTYPE.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

nm/line

Range

0.001 to 2000000.000

Default Value

20,000

Data Type

Integer

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

FB1.LINEPITCH

3500h

0ah

Unsigned32

-

1000:1

Read/Write

No

FB2.LINEPITCH

3501h

0ah

Unsigned32

-

1000:1

Read/Write

No

FB3.LINEPITCH

3502h

0ah

Unsigned32

-

1000:1

Read/Write

No

FB4.LINEPITCH

3503h

0ah

Unsigned32

-

1000:1

Read/Write

No

FB5.LINEPITCH

3504h

0ah

Unsigned32

-

1000:1

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

30380

1

30380 (0x76ac)

FB1.LINEPITCH

Unsigned32

Read/Write

Yes

30381

1

30381 (0x76ad)

FB2.LINEPITCH

Unsigned32

Read/Write

Yes

30382

1

30382 (0x76ae)

FB3.LINEPITCH

Unsigned32

Read/Write

Yes

30383

1

30383 (0x76af)

FB4.LINEPITCH

Unsigned32

Read/Write

Yes

30384

1

30384 (0x76b0)

FB5.LINEPITCH

Unsigned32

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

FB1.LINEPITCH

30380

Float

Read/Write

-

FB2.LINEPITCH

30381

Float

Read/Write

-

FB3.LINEPITCH

30382

Float

Read/Write

-

FB4.LINEPITCH

30383

Float

Read/Write

-

FB5.LINEPITCH

30384

Float

Read/Write

-