SFA#.INFO

Description

SFA#.INFO provides information about the Smart Feedback Adapter (SFA) device attached to the feedback connector.

SFA#.INFO reports the following information.

Name Description
Serial Number Unique serial number of SFA device
Part Number SFA hardware part number
Model Number SFA device model number
Installed FPGA Version FPGA version currently on the SFA
Available FGPA Version FPGA version available to download to the SFA via SFA#.UPDATE

Versions

Action Version Notes
Implemented 02-01-02-000

General Information

Type

Read Only

Description

Smart Feedback Adapter Information

Data Type

String

Variants Supported

All variants are supported.

Related Topics

Feedback Connector X41