Scaled Feedback

For feedback not associated with an axis, a set of scaled feedback parameters are provided to optionally represent the feedback position in scaled units.

The Scaled Position is calculated as follows:

FB#.SCALED.DIR Direction Sign
0 1
1 -1

Dual-Loop

There are separate feedback sources for the current, velocity, and position loops. By default they’re all set to the current loop feedback source (AXIS#.IL.FBSOURCE). If a separate feedback is desired for the different loops, those sources can be set independently using AXIS#.VL.FBSOURCE and AXIS#.PL.FBSOURCE.

Electronic Gearing

For Electronic Gearing, AXIS#.GEAR.FBSOURCE is also available. See the Electronic Gearing feature for more information.