COGCOMP.EN

Description

If the COGCOMP.EN is set to one, the current regulator will add a feedforward current depending on the actual feedback position (PL.FB) stored in the cogging compensation correction value (COGCOMP.CORRECTIONTABLE).

General Information

This content is not applicable to KAS.

Type

NV Parameter

Units

N/A

Range

0 to 1

Default Value

0

Data Type

Integer

Start Version

M_01-14-06-001

Variant Supported
MKD EtherCAT Yes
AKD-N Yes
MKD-N Yes
MKD-C No
EtherCAT CoE and CANopen
Index/Subindex Object Start Version

540Fh/0

M_01-14-06-001