COGCOMP.SAVE
Description
This parameter saves the current cogging compensation table (COGCOMP.CORRECTIONTABLE) from RAM to NV memory. On next drive boot, the cogging compensation table will be initialized with the stored entries from NV.
General Information
This content is not applicable to KAS.
Type |
Command |
Units |
N/A |
Range |
N/A |
Default Value |
N/A |
Data Type |
N/A |
Start Version |
M_01-14-07-000 |
Variant | Supported |
---|---|
MKD EtherCAT | Yes |
AKD-N | Yes |
MKD-N | Yes |
MKD-C | No |