Fieldbus - EtherCAT

Name

Description

DriveParamRead

Reads a drive parameter by sending an ASCII command to a drive.

DriveParamStrRead

Reads a single drive parameter by sending an ASCII command to a drive.

DriveParamWrite

Writes a drive parameter by sending an ASCII command to a drive.

ECATCommErrors

Returns a list of bad EtherCAT connections.

ECATDeviceAction

Performs an action on an EtherCAT device.

ECATDeviceStatus

Provides the EtherCAT state and the port link status information for the EtherCAT device.

ECATDevReadParam

Returns the EtherCAT device-specific information.

ECATGetObjVal - Deprecated

Deprecated.

ECATMasterStatus

Reads the EtherCAT master state and the lost frame counter to determine if EtherCAT is running normally.

ECATReadData

Reads cyclic parameter (byte offset format).

ECATReadPDOData

Copies the Input (Tx) PDO object data from an EtherCAT cyclic frame to a byte array.

ECATReadSdo

Reads a 32-bit word from I/O nodes using a CANopen SDO read command.

ECATReadSdoData

Reads data from an EtherCAT device using CANopen SDO read command.

ECATWCStatus

Returns the current number of working counter errors for the Sync unit.

ECATWriteData

Writes cyclic parameter (byte offset format).

ECATWritePDOData

Writes data to an Output Rx PDO object of the EtherCAT device in the cyclic EtherCAT frame.

ECATWriteSdo

Writes a 32-bit word to I/O nodes using a CANopen SDO write command.

ECATWriteSdoData

Writes data to an EtherCAT device using a CANopen SDO write command..

FSoEParamsInit

Transfers safety parameters from the safety master to safety slave devices to initialize the safety network.

Remarks

The EtherCAT SDO function blocks are activated by the CANopen over EtherCAT (CoE) protocol in a client/server mode.

  • The client (aka EtherCAT master) is the KAS Runtime application.
  • The servers (aka EtherCAT slaves) are the drives and I/O nodes where data can be retrieved.
  • The SDO function blocks only support the reading and writing of 32-bit values.
    • It is the fundamental size of CANopen SDO calls.

Why use ECATReadSdo and ECATWriteSdo FBs?

Why use the DriveParam FBs?

Reasons to prefer the DriveParam FBs are:

  • They allow direct use of the parameter name.
    • Example: IL.LIMITP instead of the SDO index: 356Eh
  • They can be used to setup a drive terminal in the HMI application.
    • This is similar to the Terminal view available in the AKD widget embedded in the KAS-IDE.

Concept Link IconSee Also