Boolean Parameters

This table is a list of Boolean supported parameters.

These parameters are read and written by the function blocks MC_ReadBoolPar and MC_WriteBoolPar.

 

1011

1013

1025

1026

1027

1033

1038

1039

Parameter Details

ID

Parameter

Name

R/W

Update Rate Type

Description

1011

MC_AXIS_PARAM_IN_POSITION

Axis In-Position

Read-only

Controller

  • TRUE if the axis:
    • Has no active or next move queued.
    • Command delta is 0 (zero).
    • Actual position is within the in-position bandwidth of the command position.
  • FALSE otherwise, Boolean.

1013

MC_AXIS_PARAM_DRIVE_WARNING

Drive Warning

Read-only

EtherCAT Cyclic

Drive Warning Status.

See Note 1.

1025

MC_AXIS_PARAM_REGIST_GOOD

Good Registration Mark Occurred

Read-only

EtherCAT Non-Cyclic

  • TRUE indicates a good registration mark was encountered.
  • This Boolean is automatically reset after it has been read.

1026

MC_AXIS_PARAM_REGIST_BAD

Bad Registration Mark Occurred

Read-only

EtherCAT Non-Cyclic

  • TRUE indicates a bad registration mark was encountered.
  • This Boolean is automatically reset after it has been read.

1027

MC_AXIS_PARAM_FI_OCCURRED

Fast Input Occurred

Read-only

EtherCAT Non-Cyclic

  • This parameter is deprecated.
  • The recommended replacement is the Done output of the MC_TouchProbe function block to verify if the fast input has occurred.

Deprecated Behavior

  • TRUE if a fast input occurred on either Capture Engine 0 or Engine 1.
  • This Boolean is automatically reset after it has been read.

1033

MC_AXIS_PARAM_APPLY_SUPERIMPOSED_DISTANCE

Apply Superimposed Distance

Read / Write

Controller

The default value for this parameter is FALSE.

  • The final reported position of the axis, which does include superimposed distance, may not be equal to the Position input to MC_MoveAbsolute.
  • The final reported position of the axis is equal to the Position input to MC_MoveAbsolute.

Note

  • When MC_MoveAbsolute begins execution, the distance to move is calculated at that point in time.
  • If a superimposed move is started while MC_MoveAbsolute is in progress, the final position of the axis when MC_MoveAbsolute completes is not equal to the Position input, regardless of the value of this parameter.

1038

MC_AXIS_PARAM_IGNORE_DRIVE_LIM_STATUS

Ignore Drive Limit Active

Read / Write

EtherCAT Non-Cyclic

  • The default value is FALSE.
  • When TRUE, the Pipe Network motion engine ignores the DS-402 Status wordbit #11 (Internal Limit Active).
  • See Overtravel Conditions.

1039

MC_AXIS_PARAM_DRIVE_OVERRIDE_ON_LIMIT_ACTIVE

Drive Override on Limit Active

Read / Write

Static

  • Set to TRUE if the drive ignores controller demand position when DS-402 Status word bit #11 (Internal Limit Active) is on.
  • Set to FALSE if the Pipe Network is responsible for stopping an axis when DS-402 Status word bit #11 is on.
  • The default value for axes connected to AKD-family drives is TRUE.
    • For all other axes, the default value is FALSE.

Notes

See Tuning Controller Performance for EtherCAT Communication Latency.

  1. This is a configuration parameter.
  2. There is some delay in acquiring fast input information from drives and calculating the registration marks.
    While the information is evaluated cyclically, there may be a few cycles between when the fast input occurs and the system records the registration marks.
  3. There is some delay in acquiring fast input information from drives and calculating the fast input position.
    While the information is evaluated cyclically, there may be a few cycles between when the fast input occurs and the system records the fast input data.
  4. There is some delay in acquiring the actual position values.
    While the information is evaluated cyclically, there may be a few cycles between when the actual position is updated in the drive and the system records the fast input data.

See Also